USB Media Transfer Protocol

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Media Transfer Protocol

1,343 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bboyd17 on Fri Mar 11 06:56:43 MST 2016
Does anyone know if the usb rom drivers are capable of supporting the media transfer protocol?

I have an application where an SDHC card will be connected to an LPC11U68, running FatFS on the processor to log data. It would be great to make the data on the SDHC card available via USB, but obviously using the mass strorage class runs into the host and local processor contending over the file system - not pretty!

The USB media transfer protocol may be a way around this, since the host is then effectively interacting with the local processor rather than directly with the file system.

Has anyone come across support for this class in LPCOpenWare?

Thanks.
标签 (1)
0 项奖励
回复
1 回复

1,284 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复