USB IAD Problem rndis + vcom on LPCxpresso54s018M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB IAD Problem rndis + vcom on LPCxpresso54s018M

2,508 Views
rijn
Contributor I

Hi there, i am attempting to run USB IAD, first device : rndis device, second device : usb vcom

 

i am able to make windows detect both device, usb rndis + usb vcom,

usb vcom is working , but usb rndis is not receiving or sending anything to me.

 

Can someone please check ?

 

0 Kudos
Reply
5 Replies

2,467 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi rijn 

How does usb rndis work if you disable USB vcom?

Thanks,

Jun Zhang

0 Kudos
Reply

2,460 Views
rijn
Contributor I

no  it does not work.

 

rndis does not work even if i disable vcom

 

0 Kudos
Reply

2,448 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Could you please test SDK demo usb_device_cdc_vnic? The purpose of this demo is to show
how to build a device of USB CDC class to implement RNDIS protocol and to provide a simple project for further development.

Thanks,

Jun Zhang

0 Kudos
Reply

2,436 Views
rijn
Contributor I

Please check demo and see if you understand my question .

i am trying to run IAD.

and RNDIS+Vcom both on one interface.

 

0 Kudos
Reply

2,425 Views
shaozhongliangs
NXP Employee
NXP Employee

@rijn 

    The attached project is a simple demonstration program based on LPC54018/SDK/usb_examples/usb_device_composite_cdc_vcom_cdc_vcom.
It is enumerated as one RNDIS network port and one virtual COM.
This demo is to show how to build a composite USB device and to provide a
simple example for further development.

   I tested the demo on WIN10. It works fine.

IDE: KEIL

HW:LPC54018 EVK + FS USB port

shaozhongliangs_0-1684933705577.png

 

shaozhongliangs_1-1684933716278.png

 

0 Kudos
Reply