USB Host example errors for LPC17xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Host example errors for LPC17xx

2,840件の閲覧回数
felipeavila
Contributor I

Hello, i'm trying to run USB Host code example provided by NXP for LPC17xx.
I have LPC1768 and I'm using the mass storage example.
I already check my board, it doesn't matter what I do I always get an error returning from "USBH_MSC_DriveGetMediaStatus" function.
USBH_Initialize returns OK.

The USB led works great, when I put a pendrive it blinks and thn stays On, and the opposite when flashdrive is removed.
Does anyone have an idea?

0 件の賞賛
返信
3 返答(返信)

2,494件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
I was wondering if you can share compile-able demo, then I can replicate the issue on my site.
I'm looking forward to your reply.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,494件の閲覧回数
felipeavila
Contributor I

Hi jeremyzhou‌ !

The example I've tested is exactly the same provided in Keil MDK5 (can be found in this software pack MDK5 - Keil MCB1700 ).

I found online another code, from uVision 4, and this one works better, what eliminates any hardware issue possibilities.

Thank you!

0 件の賞賛
返信

2,494件の閲覧回数
felipeavila
Contributor I

The error is 33 : usbDeviceError

But the USB Led is ON! Indicating that the device is detected!

0 件の賞賛
返信