USB HID Keyboard example for lpc1343

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB HID Keyboard example for lpc1343

3,779 Views
jldesigns
Contributor I

Can anyone point me to example for using USB HID Keyboard on lpc1343? I can see an example for lpc1347, lpc11u14, lpc1768, but nothing for lpc1343. 

Labels (2)
0 Kudos
Reply
3 Replies

2,893 Views
jldesigns
Contributor I

Thank you, but it does not provide example how to implement hid device descriptors to use it as a keyboard, joystick or mouse.

You had some examples on that before, but its not on sites anymore. 

Is lpc1343 going in to stage were its not supported anymore?

0 Kudos
Reply

2,892 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Hot Dog

I found this old sample that one customer share us, please check it.

I hope this will help you.Regards

Vicente Gomez

0 Kudos
Reply

2,892 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jakub,

You could use the following Application note as referece, it explains how to use the on-chip USB drivers in the LPC1300 Cortex-M3 based microcontroller to implement a simple USB Human Interface Device (HID):

http://cache.nxp.com/documents/application_note/AN10904.zip


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply