USB HID Keyboard example for lpc1343

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB HID Keyboard example for lpc1343

3,786件の閲覧回数
jldesigns
Contributor I

Can anyone point me to example for using USB HID Keyboard on lpc1343? I can see an example for lpc1347, lpc11u14, lpc1768, but nothing for lpc1343. 

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,900件の閲覧回数
jldesigns
Contributor I

Thank you, but it does not provide example how to implement hid device descriptors to use it as a keyboard, joystick or mouse.

You had some examples on that before, but its not on sites anymore. 

Is lpc1343 going in to stage were its not supported anymore?

0 件の賞賛
返信

2,899件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Hot Dog

I found this old sample that one customer share us, please check it.

I hope this will help you.Regards

Vicente Gomez

0 件の賞賛
返信

2,899件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jakub,

You could use the following Application note as referece, it explains how to use the on-chip USB drivers in the LPC1300 Cortex-M3 based microcontroller to implement a simple USB Human Interface Device (HID):

http://cache.nxp.com/documents/application_note/AN10904.zip


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信