USB Device : VCOM stop working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Device : VCOM stop working

2,066 Views
riteshunde
Contributor I

Hi,

I am using OM13092 LPCXpresso with LPC54608. While using MCUxpresso with USB example usb_device_cdc_vcom, it was working fine with echo back of byte I was transmitting on port.but suddenly it stopped working. I can view VCOM port in device driver but it doesn't echo back any data.

I tried with following options :

1. Reinstalling vcom port driver

2. Reinstalling MCUXpresso IDE v10.0.0

3. Swapping USB ports on PC

I am using Windows 7 professional, 32 bit OS.

0 Kudos
Reply
2 Replies

1,869 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ritesh unde,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
I was wondering if you can introduce the steps to replicate the issue.
I'm looking forward to your reply.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,869 Views
riteshunde
Contributor I

Hi @jeremyzhou,

Solved, there were some com0 drivers installed on my pc, removed those and vcom started to work.

Thanks.

0 Kudos
Reply