USB Composite Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Composite Device

1,341件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vamshig51 on Thu Jun 09 21:36:12 MST 2016
Dear Team,

I understand from the data sheet UM10430 that USB-0 & USB-1 supports as a composite device, and we have to use the drivers implemented in the Boot ROM for enabling the same. Please correct me If I am wrong.

Composite device I am looking for is HID Keyboard + Mouse

For configuring a USB controller in device mode (composite device) what are the minimum number of end-points need, I assume still we need only one control end-point. <correct me if I am wrong>

If any sample code for Composite device please give me pointers.


Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,262件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信