USB Composite Device(MSC+HID) ,OH my god

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Composite Device(MSC+HID) ,OH my god

2,174件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by free_soul on Sun Oct 21 19:54:33 MST 2012
USE LPC11UXX 
on chip-drivers , Only one device function can be used by the application software?????

USB Composite Device(MSC+HID), how to do it????(on chip-drivers)

ラベル(1)
  • USB

0 件の賞賛
返信
2 返答(返信)

1,995件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tsuneo on Mon Oct 22 06:15:33 MST 2012
The on-chip USB drivers of LPC11Uxx share the common interface with LPC1347's.
We have discussed on composite devices (HID + CDC, HID + HID) using the on-chip driver at this LPCXpresso topic. MSC+HID also is made in similar way.

USB Composite Device on LPC1347
http://www.lpcware.com/showthread.php?t=3659

Tsuneo
0 件の賞賛
返信

1,995件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by free_soul on Mon Oct 22 01:43:58 MST 2012
@@@@@@@@@@@nxpUSBlib team 
0 件の賞賛
返信