USB Composite Device(MSC+HID) ,OH my god

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Composite Device(MSC+HID) ,OH my god

1,745 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by free_soul on Sun Oct 21 19:54:33 MST 2012
USE LPC11UXX 
on chip-drivers , Only one device function can be used by the application software?????

USB Composite Device(MSC+HID), how to do it????(on chip-drivers)

Labels (1)
0 Kudos
Reply
2 Replies

1,566 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tsuneo on Mon Oct 22 06:15:33 MST 2012
The on-chip USB drivers of LPC11Uxx share the common interface with LPC1347's.
We have discussed on composite devices (HID + CDC, HID + HID) using the on-chip driver at this LPCXpresso topic. MSC+HID also is made in similar way.

USB Composite Device on LPC1347
http://www.lpcware.com/showthread.php?t=3659

Tsuneo
0 Kudos
Reply

1,566 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by free_soul on Mon Oct 22 01:43:58 MST 2012
@@@@@@@@@@@nxpUSBlib team 
0 Kudos
Reply