USART send/receive on same wire (One-Wire UART) — why is RX not triggering despite valid waveform on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USART send/receive on same wire (One-Wire UART) — why is RX not triggering despite valid waveform on

1,315 Views
cclark
Contributor I

I’m working on a One-Wire UART setup using the LPC54114, where TX and RX share the same physical wire. The idea is to implement Maxim’s timing trick by sending a 0xFF byte and checking what’s received back to detect if the slave is pulling the line low. This approach follows the method shown in this screenshot from Analog Devices’ “Implementing One-Wire with UART” application note.

https://www.analog.com/en/resources/technical-articles/using-a-uart-to-implement-a-1wire-bus-master....

Setup:

TX is connected through a 1kΩ resistor to a shared bus line. RX is connected directly to the same node as the TX output and the One-Wire slave. The bus is pulled up to 3.3V. The slave is working correctly (verified with GPIO bit-banged One-Wire). Baud rate is 115200, 8N1. Using MCUXpresso SDK APIs: USART_Init(), USART_TransferSendNonBlocking(), USART_TransferReceiveNonBlocking(), with a configured handle.

What I expect: 1.Transmit 0xFF onto the bus. 2.USART RX should sample the response. If the line stays high, RX should read 0xFF. If a slave pulls low briefly, RX should return something like 0xFD or 0x00 depending on how many bits were pulled low.

What’s happening:

TX waveform looks perfect on the oscilloscope. RX pin sees the same waveform (confirmed on the shared node with TX and slave). But the RX FIFO never fills, and the RX callback never fires. Calling USART_TransferReceiveNonBlocking() before or after transmit doesn’t help. Internal loopback mode also works, but that bypasses the actual RX pin.

What I’ve tried:

Confirmed IOCON pinmux and Flexcomm PSELID. Tried both with and without ring buffer. Tried manually flushing the FIFO and reinitializing after each transfer. Tried calling send/receive in both orders with various timing gaps. Tested multiple Flexcomm instances. Scoped the signals — waveform is clean and timings look correct.

What I need:

A working SDK example or explanation for using TX and RX on the same USART wire using MCUXpresso APIs. Insight into why RX doesn’t trigger even with a valid waveform. Clarification on whether there are FIFO or sampling constraints that could be preventing the USART from recognizing the RX data.

Happy to provide scope captures, code snippets (init and transfer logic), or pin configs if anyone’s willing to dig in.

Really appreciate any help — I feel like I’m 90% of the way there, but something critical is being missed.

Labels (2)
0 Kudos
Reply
1 Reply

1,247 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @cclark 

There are some points that need to be checked:

 

  1. Please configure it for normal operation, not loopback mode.

Alice_Yang_0-1753690669000.png

2. Please disable Receive(RX) before Send (TX).

3. Connect to the open-drain bus.

 

BR

Alice

0 Kudos
Reply