USART_TransferReceiveNonBlocking not receiving the data on LPC55S69

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USART_TransferReceiveNonBlocking not receiving the data on LPC55S69

2,916 次查看
sushmasan
Contributor II

Hello Team,

This is regarding USART communication between a device (Example: Raspberry Pi) and LPC55S69 using Flexcomm2 interface.

I checked different sdk examples, and implemented my application in the similar manner, but still my application is not working as expected.

I have followed these steps,

I have Configured the relevant GPIO's (PIO1_24 as RX and PIO1_25 as TX) as given below

CLOCK_EnableClock(kCLOCK_Iocon);
CLOCK_EnableClock(kCLOCK_Gpio1);

// gpio_port_num=1, gpio_pin_num=24/25, gpio_pin_alt_func=0x01, enable_digital = 0x01
IOCON->PIO[gpio_port_num][gpio_pin_num] = ((IOCON->PIO[gpio_port_num][gpio_pin_num] &
					/* Mask bits to zero which we are setting */
					(~(IOCON_PIO_FUNC_MASK | IOCON_PIO_DIGIMODE_MASK)))

					| IOCON_PIO_FUNC(gpio_pin_alt_func)

					| IOCON_PIO_DIGIMODE(enable_digital));

 

Get the default configuration,

USART_GetDefaultConfig(&usart2_config);
usart2_config.baudRate_Bps = 921600U;
usart2_config.enableTx = false;
usart2_config.enableRx = true;
usart2_config.parityMode = kUSART_ParityDisabled;
usart2_config.stopBitCount = kUSART_OneStopBit;

Invoke uart init

// #define USART_IF2 USART2
USART_Init(USART_IF2, &usart2_config, CLOCK_GetFlexCommClkFreq(2U));

Create uart handle

USART_TransferCreateHandle(USART_IF2, &g_uartHandle, USART2_UserCallback, NULL);

 

Define receive buffer,

// #define BUFFER_SIZE 256
receiveXfer.data = receiveBuffer;
receiveXfer.dataSize = BUFFER_SIZE;

Invoke the non-blocking receive call,

if ((!rxOnGoing) && rxBufferEmpty)
{
	USART_TransferGetReceiveCount(USART_IF2, &g_uartHandle, &rx_count); 	
	USART_TransferReceiveNonBlocking(USART_IF2, &g_uartHandle, &receiveXfer, &receivedBytes);
}

When the above two functions are invoked in a while loop, then only I am seeing the data count (USART_TransferGetReceiveCount gives the correct data count).

Let's say Raspberry Pi is sending 10 bytes of data, USART_TransferGetReceiveCount  is giving 10 bytes, but "USART_TransferReceiveNonBlocking" does not contain any data in the receive buffer.

Where as when the above two functions are invoked one time, there is no data count (zero) also seen.

The callback is defined like this,

void USART2_UserCallback(USART_Type *base, usart_handle_t *handle, status_t status, void *userData)
		{
			if (kStatus_USART_RxIdle == status || status == kStatus_Success)
			{
				PRINTF("status is kStatus_USART_RxIdle \r\n");
				rxBufferEmpty = false;
				rxOnGoing     = false;
			}
		}

 

In the call back, the control never reached to this condition.
kStatus_USART_RxIdle == status || status == kStatus_Success

Can someone please let me know, what I am missing here?

Regards,
San

 

0 项奖励
回复
6 回复数

2,854 次查看
sushmasan
Contributor II

Hello,

 

Can someone please respond my question?

 

Regards,
San

0 项奖励
回复

2,771 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sushmasan 

 
I recommend that you first use the UART demo under the SDK for testing to rule out issues with other devices.
 
BR
Alice
0 项奖励
回复

2,749 次查看
sushmasan
Contributor II

Hello @Alice_Yang ,

Thanks for your response.

Before even posting this question, I tried all other possibilities (like trying with SDK examples between two EVK's) those examples working fine. But when it comes to testing with Rpi and I am seeing an issue.

Anyway I will check it from my end.

Regards,
Santhosh

 

0 项奖励
回复

2,729 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sushmasan 

 

Please use a logic analyzer to capture waveforms for analysis and figure out where the problems is in the communication process.

 

BR

Alice

0 项奖励
回复

2,724 次查看
sushmasan
Contributor II

Hello @Alice_Yang ,

Okay, I will check.

Regards,
San

0 项奖励
回复

2,912 次查看
sushmasan
Contributor II

Small correction in my previous message,

USART_TransferReceiveNonBlocking(USART_IF2, &g_uartHandle, &receiveXfer, &receivedBytes);
USART_TransferGetReceiveCount(USART_IF2, &g_uartHandle, &rx_count); 	

please note that this is the order the functions are invoked. 

0 项奖励
回复