USART AT Command/Response Parser

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USART AT Command/Response Parser

1,535件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Tue Jul 16 09:50:48 MST 2013
Hey guys. This isn't an LPC specific question, but what's the best way to communicate with an AT command driven device (In this case a PAN1721 with BlueRadios firmware)through the USART? I've written lots of low-level drivers for i2c or SPI devices, but this one's got strings, and parsing, and unsolicited event notifications, the works... I need to figure out a way to build an API around all this stuff so my main application can call things like PAN1721_GetAddress(), PAN1721_Scan(), PAN1721_Connect(), etc. Any help would be appreciated, as I'm not sure where to even start...
ラベル(1)
0 件の賞賛
返信
0 返答(返信)