UM10430 Fan PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UM10430 Fan PWM

1,620件の閲覧回数
Kushal_Panchal
Contributor II

When i set the PWM zero it increasing the fanspeed it working fine above 20 pwm .

0 件の賞賛
返信
2 返答(返信)

1,582件の閲覧回数
Kushal_Panchal
Contributor II

Thanks for your reply.

Yes its help me to resolve my problem.

Regards,

kushal

0 件の賞賛
返信

1,605件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use LPC1800 family, it has MotorCONPWM module, you use it to control motor.

Can you tell us the motor type you are using? do you control BLDC, PMSM or DC motor?

If you control a DC motor with a bipolar switching mode, it is possible to that you set the PWM duty cycle to zero, the DC motor speed will increase. In the bipolar switching mode, if you set the duty cycle of PWM in 50%, the DC motor will stall.

Hope it can help you

BR

XiangJun Rong