UM10430 Fan PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UM10430 Fan PWM

1,616 Views
Kushal_Panchal
Contributor II

When i set the PWM zero it increasing the fanspeed it working fine above 20 pwm .

0 Kudos
Reply
2 Replies

1,578 Views
Kushal_Panchal
Contributor II

Thanks for your reply.

Yes its help me to resolve my problem.

Regards,

kushal

0 Kudos
Reply

1,601 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use LPC1800 family, it has MotorCONPWM module, you use it to control motor.

Can you tell us the motor type you are using? do you control BLDC, PMSM or DC motor?

If you control a DC motor with a bipolar switching mode, it is possible to that you set the PWM duty cycle to zero, the DC motor speed will increase. In the bipolar switching mode, if you set the duty cycle of PWM in 50%, the DC motor will stall.

Hope it can help you

BR

XiangJun Rong