UM10360 Modem Control Register explanation might be incorrect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UM10360 Modem Control Register explanation might be incorrect

1,260件の閲覧回数
nakano-r
Contributor I

Hi, there.

UM10360 Chap.15 page338

"If Auto-RTS mode is disabled, the RTSen  bit controls the RTS1 output of the UART1...."

I think RTSen bit is not correct, because RTSen bit dedicated to enable or disable flow control. I guess "RTS Control bit" is correct.

Am I right? Please follow me.

ラベル(1)
0 件の賞賛
返信
1 返信

1,190件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rick nack ,

Yes, you are right , it may be a typo in UM.

   

" If Auto-RTS mode is disabled, the RTSCTRL bit controls the RTS1 output of the UART1.

Hope it helps,

 

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信