UM10360 Modem Control Register explanation might be incorrect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UM10360 Modem Control Register explanation might be incorrect

1,320 次查看
nakano-r
Contributor I

Hi, there.

UM10360 Chap.15 page338

"If Auto-RTS mode is disabled, the RTSen  bit controls the RTS1 output of the UART1...."

I think RTSen bit is not correct, because RTSen bit dedicated to enable or disable flow control. I guess "RTS Control bit" is correct.

Am I right? Please follow me.

标签 (1)
0 项奖励
回复
1 回复

1,250 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello rick nack ,

Yes, you are right , it may be a typo in UM.

   

" If Auto-RTS mode is disabled, the RTSCTRL bit controls the RTS1 output of the UART1.

Hope it helps,

 

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复