UART0 DMA PROBLEM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART0 DMA PROBLEM

1,458件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by salamlora1 on Sun Aug 25 00:21:00 MST 2013
Hi all
i right a program for UART0 whit DMA it’s not work correctly any one can fine my mistake ???
  



#include <nxp/iolpc1768.h>
#include <stdio.h>
#include "gpio1768.h"
unsigned char h[]="1";
char a[2]="11";
void uart_init(unsigned short baud)
{
  unsigned short div;                                                 //PCONP |= 0x20210048 ;
  CLKOUTCFG = 0;
  div = (unsigned short)(10000000/(baud*16L));
  U0LCR = 0x83;
  U0DLL = (div);
  U0DLM = (div>>8);
  U0LCR &= ~(1<<7);
  PINSEL0 |= (1<<4);
  //U0FCR = 0x87;/* Enable and reset TX and RX FIFO. */
  U0FCR |= 0x87;
 
}

void dmacon(void)
{
  U0FCR = 0x87;
  PCONP = 0xffffffff;
  CCLKCFG = 0;
  PCONP |=(1<<29);
  DMACCONFIGURATION = 0x00000001;
  DMACC0CONFIGURATION = 0x00000001;
  DMACINTTCCLEAR = 0xff ;    //clear all interrupts
  DMACINTERRCLR = 0xff;  //eclear interrupt errors
  DMACC0SRCADDR = ( int ) &a;
  DMACC0DESTADDR = ( int ) &U0THR;
  DMACC0LLI =0;//(unsigned int ) &a[1];
  DMACC0CONTROL = sizeof(a);
  DMACC0CONTROL |= (1<<12);
  DMACC0CONFIGURATION |= (1<<0);
  DMACC0CONFIGURATION |= (1000<<6);
  DMACC0CONFIGURATION |= (1<<11);
  DMACC0CONFIGURATION |= 0x00000001;
  //delay(50000);
         
}
// PLL INIT

void pllinit (void)
{
//((FCCO = (2 × M × FIN) / N))
//"M" is bit of 14:0  PLL0CFG and "N" is bit of 23:16
        SCS = (0x00000001 << 5);          //Enable Main Oscillator
        SCS |= 0x00000020;                //Select the main Oscillator range
        PLL0CON &= ~0x01;                 //Disconnect the PLL
        PLL0FEED = 0xAA;
        PLL0FEED = 0x55;
        PLL0CON &= ~0x01;                 //Disconnect the PLL
        PLL0FEED = 0xAA;
        PLL0FEED = 0x55;                  //Write feed sequence
        while(!(SCS & 0x00000040));       //Wait untill Main Oscillator is stable
        CLKSRCSEL = 0x00000001;           //Select Main Oscillator as PLL Imput
        PLL0CFG = (0x000000A|0x00020000); //Write PLL Multipiler and Divider values
        PLL0FEED = 0xAA;
        PLL0FEED = 0x55;                  //Write Feed Sequence
        PLL0CON = 0x01;                   //Enable PLL
        PLL0FEED = 0xAA;
        PLL0FEED = 0x55;                  //Wriete Feed Sequence
        USBCLKCFG = 0x00000009;           //Write USBSEL Divider value
        CCLKCFG = 0x00000008;             //Write CPU Divider Value
        while(PLL0STAT & 0x000);          //Wait PLL for Lock
        PLL0CON |= 0x02;                  //Connect the PLL
        PLL0FEED = 0xAA;
        PLL0FEED = 0x55;
}
void main()
{ dmacon();
  U0TER = 0x80;
  U0FCR = 0x1;
  U0FCR = 0x87;
  pllinit();
  //dir0(24);
  //set0(24) ;
// PCLKSEL0 |=(1<<6);       //pish taghsim konanad e PCLK
  uart_init(9600);
  //delay(500);
  //delay(500);
//U0THR = '0';
//U0THR = '1';
//U0THR = '2';
//U0THR = '3';
//U0THR = '4';

  //U0FCR |=(1<<0);
  //U0FCR |=(1<<1);
  U0TER |= 0x80;
  while (1)
{
    delay(2);
    while( (U1LSR & (1<<5))== 0);
    uart_init(9600);
    U0TER = 0x80;
    dmacon();
    delay(10000) ;
}

}
ラベル(1)
0 件の賞賛
返信
1 返信

1,423件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by salamlora1 on Mon Aug 26 22:07:37 MST 2013
??????   :((
0 件の賞賛
返信