UART not working (at all!)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART not working (at all!)

1,607件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by klemikaze on Tue May 03 11:22:17 MST 2016
Hi.
I have ConnectBlue OEMSPA310 Bluetooth module connected to LPC 1769 P0[15] / P0[16] pins. When I run LPC Open periph_uart_rb project, it should send two messages. As the project originally uses UART0, I changed those define statements to use UART1, otherwise the project isn't modified.

#define UART_SELECTION LPC_UART1
#define IRQ_SELECTION UART1_IRQn
#define HANDLER_NAME UART1_IRQHandler



/* Send initial messages */
Chip_UART_SendRB(UART_SELECTION, &txring, inst1, sizeof(inst1) - 1);
Chip_UART_SendRB(UART_SELECTION, &txring, inst2, sizeof(inst2) - 1);


but I am not able to catch them in my computer. Also, I am not able to capture packet sent from my PC. Could you please troubleshoot my problem? I don't have any other ideas of how to "debug" (or how to correctly connect) this issue and no other threads describe such issue, all solve characters mismatches and timeouts, but I just don't receive anything.

As the readme in project says
Quote:
The terminal program on the host PC should be setup for 115200-8-N-1.

which I have done both in my desktop app, Tera Term and finally serial port settings.

Any help will be greatly appreciated.
ラベル(1)
0 件の賞賛
返信
1 返信

1,476件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信