UART example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART example

1,874 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dudush on Tue Dec 25 07:26:27 MST 2012
i'm using mcb4350 board with keil and i didn't succeed to send/receive any data from the uart examples(i'm using the lpc43xx libraries).
I really appreciate if somebody send we a code example (just to send/receive data)or offer me another solution.

Labels (1)
0 Kudos
Reply
1 Reply

1,831 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp21346 on Wed Dec 26 10:48:47 MST 2012
Hi!

Did you try the CMSIS/PDL examples or the LPCOpen Platform?
Did the code compile and download to the board OK?
Can you step through and debug it?
Also: Did you know that there is a set of jumpers on the Keil mcb4350 board which can select UART output on UART0 or on UART3?

Thanks,
-Dave @ NXP
0 Kudos
Reply