UART+DMA to transfer unequal ength data packet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART+DMA to transfer unequal ength data packet

1,668件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi Team,

One of my cusomter is using LPC54605, in their applications, they will use high speed UART, the baud rate will up to 2Mbps, they need to use UART+DMA to transfer data, and the length of frame are difference, do you have any suggestion for DMA to receive unequal length data packets? Thanks.

Best Regards,

Fred Fu

ラベル(2)
0 件の賞賛
返信
1 返信

1,542件の閲覧回数
bin_er
NXP Employee
NXP Employee

I would adding a header + packet length for the data sent and application can concatenate the data next. I may not propose for DMA transmission for unequal length data.

The DMA descriptor and memory buffer is easy managed for fixed length transfer + backend data concatenation.

0 件の賞賛
返信