UART 1: equipped with standard modem interface signals.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART 1: equipped with standard modem interface signals.

1,752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SURESH BABU K on Sat Feb 21 02:23:27 MST 2015
hi,

    how to use UART 1 as a Modem interface and what are the applications. can i have sample KEIL MDK ARM project.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,730件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SURESH BABU K on Thu Mar 05 02:39:23 MST 2015
Thanks for your reply, so please guide me how to send data from one modem to other.
0 件の賞賛
返信

1,730件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Mar 04 08:20:54 MST 2015
Hi SURESH BABU K,

UART historically was the protocol used for modems because it had the pins that fit the modem specifications (CTS, RTS, DSR, DTR, etc.). Nowadays, UART used on our MCUs are mainly for data transfer due to its simplicity. Do you actually want to use our MCU to interface with a modem? i don't believe we have code for that, but we do have UART sample code to send and receive data. Check our LPCOpen software platform:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc17xx-packages
0 件の賞賛
返信

1,730件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SURESH BABU K on Wed Mar 04 04:40:55 MST 2015

Quote: SURESH BABU K
hi,

    how to use UART 1 as a Modem interface and what are the applications. can i have sample KEIL MDK ARM project.


0 件の賞賛
返信