U8glib: LCD and OLED graphics library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U8glib: LCD and OLED graphics library

2,579件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by olikraus on Fri Oct 04 15:54:20 MST 2013
Hi All

The graphics library U8glib has been ported to Cortex-M0 controller. The ARM version of U8glib includes examples for NXP LPC1114 and NXP LPC1226 controller.

Project URL: http://code.google.com/p/u8glib/

[list]
  [*] Low RAM usage
  [*] Support for many LCD/OLED controller (SSD1306, SSD1325, ST7565, ST7920, UC1610, UC1701, ...)
[/list]

Oliver
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,881件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by olikraus on Wed Jul 09 21:50:09 MST 2014
Yes, but need to update the hardware abstraction layer for the 176x controller. In the 1114 example, locate file common/u8g_arm.c. This file needs to be updated. Also see INSTALL.TXT.

Another user has provided also this: http://blog.bastelhalde.de/?p=759

Oliver
0 件の賞賛
返信

1,881件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dandumit on Wed Jul 09 07:43:46 MST 2014
Hello Oliver,
could it be used for 176x ?
Kind REgards,
Daniel
0 件の賞賛
返信