U0_RTS - driving RS485

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U0_RTS - driving RS485

1,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wojtkingson on Tue Feb 10 11:16:50 MST 2015
Hi,

I want to drive my RS485 transceiver by U0_RTS, I´ve managed it by software, but I would like to do it by hardware.

Some of my steps:

Chip_SWM_MovablePinAssign(SWM_U0_RTS_O, 1);

Chip_UART_ConfigData(LPC_USART0, UART_CFG_DATALEN_8 | UART_CFG_PARITY_NONE | UART_CFG_STOPLEN_1 | UART_CFG_LOOP);



This code works fine but I cant receive anything from UART. Whenever I remove UART_CFG_LOOP, U0_RTS on PIO_01 doesn´t work anymore. I´ve tried lot of variations, but still without succes. Signal si controlled by oscilloscope, so there is problem only with pin with U0_RTS signal (I think).
Labels (1)
0 Kudos
Reply
2 Replies

1,505 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wojtkingson on Mon Mar 16 02:31:10 MST 2015
Hi,

thanks for reply. I´ve checked state of DIR/RTS pin (pin which should control TX/RX) with oscilloscope and it didn´t work. I guess, that problem is somewhere in my setting.
0 Kudos
Reply

1,505 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ramniraj10 on Sun Mar 15 22:14:31 MST 2015
Dear Wojtkingson ,

Have you checked the DIR pin of RS485 trans-reciever ic.

You an check the conenctions of RS485 in internet as how it works.
This DIR pin is ued to set up the trans receiver in Tx or Tx mode.

Thanks,
Niraj Ram
0 Kudos
Reply