Typo in the LPC802 user manual.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Typo in the LPC802 user manual.

1,810 Views
drsmith_yorku
Contributor III

Typo_CTIMER0_UserManual.PNGThe CTIMER section of the user manual for the LPC802 has a typo.  It should be PRESETCTRL0 not 1.  Seems to be confirmed in Table 64, as well as in the lpc802.h header file, so that resetting should look like this, I believe:

    // Reset the CTIMER module via PresetControl 0 register
    // bit is 1 out of reset (cleared reset).  Make it 0, then 1.
    SYSCON->PRESETCTRL0 &= ~(SYSCON_PRESETCTRL0_CTIMER0_RST_N_MASK); // 0
    SYSCON->PRESETCTRL0 |=  (SYSCON_PRESETCTRL0_CTIMER0_RST_N_MASK); // 1

Labels (2)
1 Reply

1,391 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi James,

I think you are right. I will escalate it to document to have it fixed.

Thanks you for bringing the problem to our attention.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------