Trying to get emWin running on Hitex LPC1850 EVA-Board with EA LCD-Board 7"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trying to get emWin running on Hitex LPC1850 EVA-Board with EA LCD-Board 7"

754件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Mon May 27 04:18:21 MST 2013

Hello,


I'm trying to get the emWin BSP 5.20 for the EA 1788 Dev-Kit running on my Hitex LPC1850 EVA-Board. Both Boards uses the same Display: EA 7" LCD-Board. Now I have made the modifications in the BSP. The problem is that I can't download the project in the external flash (SST39VF3201).


My IDE is Code Red RedSuite 5.


I get the following error messages:


-> Flash Driver "Init" return error code 0x1 ;


-> Target reported errors, reason:15: Target error from commit flash write ;


-> Error in final launch sequence Failed to execute MI command: -break-insert -t main
    Error Message from debugger back-end: cannot access memory at address 0x1c001f78


The parallel flash ram uses the same lines as the sdram. Could it be, that I have to switch between the memories? Did anybody have experiences with the Hitex EVAL Board and the usage of both memories? After building the Project I get an error: "make:***[NXP_Hitex1850_BSP_LPCXpresso510.axf] Error 1".


Please, can somebody help me with this problem?


Thanks.


Martin

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

730件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rgledhill on Tue Jun 18 00:57:38 MST 2013

Have you looked in the QuickStart guide for this board?  It mentions in there how to set up programming external flash...

0 件の賞賛
返信

730件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Mon May 27 22:53:21 MST 2013

I tried to program a simple Code on the external flash to check if everything is still working and I got the same error... < Flash Driver "Init" return error code 0x1 > Could it be that I damaged the external flash? 

0 件の賞賛
返信