TouchGFX NXP LPC54608 SDK error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TouchGFX NXP LPC54608 SDK error

6,542件の閲覧回数
taisenzhuang
Contributor I

I am following the document guidance from TouchGFX, downloaded SDK, which comes one library:

SDK_2.2_LPCXpresso54608

The library always this error:

libfsl_power_lib_softabi.a(fsl_power_lib.o) uses VFP register arguments, application.axf does not

the softabi SHOULD using software floating point, not hard floating point, but why still give this error??

There are two libraries in the SDK folder, one is libfsl_power_lib_softabi.a another is libfsl_power_lib.a

I believe, the libfsl_power_lib_softabi.a is soft_abi and libfsl_power_lib.a is hard abi, is that right?

here is my error:

c:/nxp/mcuxpressoide_10.0.2_411/ide/tools/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: error: C:\Users\TZ\mcuxpresso\SDKPackages\SDK_2.2_LPCXpresso54608\devices\LPC54608\mcuxpresso\libfsl_power_lib_softabi.a(fsl_power_lib.o) uses VFP register arguments, application.axf does not
SRAMX: 0 GB 32 KB 0.00%
c:/nxp/mcuxpressoide_10.0.2_411/ide/tools/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file C:\Users\TZ\mcuxpresso\SDKPackages\SDK_2.2_LPCXpresso54608\devices\LPC54608\mcuxpresso\libfsl_power_lib_softabi.a(fsl_power_lib.o)
USB_RAM: 0 GB 8 KB 0.00%
collect2.exe: error: ld returned 1 exit status

0 件の賞賛
返信
2 返答(返信)

1,884件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

A new version of the SDK package for LPC546xx is being released this week that should correct this issue. Look out for update notifications from your login on mcuxpresso.nxp.com.

1,884件の閲覧回数
taisenzhuang
Contributor I

Great, thanks for NXP team's Great effert! I will download the new SDK and try this out! 

0 件の賞賛
返信