TouchGFX 4.8.0, LPCXpresso54608 not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TouchGFX 4.8.0, LPCXpresso54608 not working

跳至解决方案
3,345 次查看
mirko_mancin
Contributor I

Hi, I have a problem when try to flash a program on this board. I have downloaded last bsp of 54608 from touchgfx site, 4.8.0 version of it, MCUXpresso and its sdk. I have create simple application with TouchGFX designer and if I try to run into simulator I haven't problem. But, if I generate code and try to open application in MCUXpresso I can't build it. I received error on fsl_power library during link.

Building target: application.axf
Invoking: MCU C++ Linker
arm-none-eabi-c++ -nostdlib -L"C:\Users\M\mcuxpresso\SDKPackages\SDK_2.2_LPCXpresso54608_MCUxpresso\devices\LPC54608\mcuxpresso" -L"C:\touchgfx\4.8.0\touchgfx\lib\core\cortex_m4f\gcc" -Xlinker -Map="application.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -mthumb -T "application_Debug.ld" -o "application.axf" ./board/board.o ./board/clock_config.o ./board/fsl_lcd_RK043.o ./board/fsl_phy.o ./board/fsl_spifi_54608_eval_board.o ./board/fsl_touch_ft5406.o ./board/leds.o ./board/pin_mux.o ./TouchGFXPort/OS/OSWrappers.o ./TouchGFXPort/MCU/CortexMMCUInstrumentation.o ./TouchGFXPort/MCU/NXP546XDMA.o ./TouchGFXPort/MCU/NXP546XHAL.o ./TouchGFXPort/Board/source/bsp/FT5336GQQTouchController.o ./TouchGFXPort/Board/source/BoardConfiguration.o ./TouchGFXPort/Board/source/GPIO.o ./OS/freertos_9.0.0-Source/portable/MemMang/heap_4.o ./OS/freertos_9.0.0-Source/portable/GCC/ARM_CM4F/fsl_tickless_systick.o ./OS/freertos_9.0.0-Source/portable/GCC/ARM_CM4F/port.o ./OS/freertos_9.0.0-Source/croutine.o ./OS/freertos_9.0.0-Source/event_groups.o ./OS/freertos_9.0.0-Source/list.o ./OS/freertos_9.0.0-Source/queue.o ./OS/freertos_9.0.0-Source/tasks.o ./OS/freertos_9.0.0-Source/timers.o ./LPC54608/utilities/fsl_debug_console.o ./LPC54608/mcuxpresso/startup_LPC54608.o ./LPC54608/drivers/fsl_adc.o ./LPC54608/drivers/fsl_clock.o ./LPC54608/drivers/fsl_common.o ./LPC54608/drivers/fsl_dma.o ./LPC54608/drivers/fsl_emc.o ./LPC54608/drivers/fsl_enet.o ./LPC54608/drivers/fsl_flexcomm.o ./LPC54608/drivers/fsl_fmc.o ./LPC54608/drivers/fsl_gpio.o ./LPC54608/drivers/fsl_i2c.o ./LPC54608/drivers/fsl_i2c_dma.o ./LPC54608/drivers/fsl_i2c_freertos.o ./LPC54608/drivers/fsl_inputmux.o ./LPC54608/drivers/fsl_lcdc.o ./LPC54608/drivers/fsl_power.o ./LPC54608/drivers/fsl_reset.o ./LPC54608/drivers/fsl_rtc.o ./LPC54608/drivers/fsl_sctimer.o ./LPC54608/drivers/fsl_spi.o ./LPC54608/drivers/fsl_spi_dma.o ./LPC54608/drivers/fsl_spi_freertos.o ./LPC54608/drivers/fsl_spifi.o ./LPC54608/drivers/fsl_spifi_dma.o ./LPC54608/drivers/fsl_usart.o ./LPC54608/drivers/fsl_usart_dma.o ./LPC54608/drivers/fsl_usart_freertos.o ./LPC54608/system_LPC54608.o ./Application/main/main.o ./Application/gui/src/screen1_screen/Screen1Presenter.o ./Application/gui/src/screen1_screen/Screen1View.o ./Application/gui/src/model/Model.o ./Application/gui/src/common/FrontendApplication.o ./Application/generated/texts/src/Texts.o ./Application/generated/texts/src/TypedTextDatabase.o ./Application/generated/images/src/__designer/Blue_Buttons_Round_Edge_small.o ./Application/generated/images/src/__designer/Blue_Buttons_Round_Edge_small_pressed.o ./Application/generated/images/src/BitmapDatabase.o ./Application/generated/gui_generated/src/screen1_screen/Screen1ViewBase.o ./Application/generated/gui_generated/src/common/FrontendApplicationBase.o ./Application/generated/fonts/src/ApplicationFontProvider.o ./Application/generated/fonts/src/FontGetters.o ./Application/generated/fonts/src/Font_verdana_10_4bpp.o ./Application/generated/fonts/src/Font_verdana_20_4bpp.o ./Application/generated/fonts/src/Font_verdana_40_4bpp.o ./Application/generated/fonts/src/Kerning_verdana_10_4bpp.o ./Application/generated/fonts/src/Kerning_verdana_20_4bpp.o ./Application/generated/fonts/src/Kerning_verdana_40_4bpp.o ./Application/generated/fonts/src/Table_verdana_10_4bpp.o ./Application/generated/fonts/src/Table_verdana_20_4bpp.o ./Application/generated/fonts/src/Table_verdana_40_4bpp.o -lfsl_power_lib_softabi -ltouchgfx
Memory region Used Size Region Size %age Used
PROGRAM_FLASH: 97876 B 512 KB 18.67%
c:/nxp/mcuxpressoide_10.0.0_344/ide/tools/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: error: C:\Users\M\mcuxpresso\SDKPackages\SDK_2.2_LPCXpresso54608_MCUxpresso\devices\LPC54608\mcuxpresso\libfsl_power_lib_softabi.a(fsl_power_lib.o) uses VFP register arguments, application.axf does not
SPIFI: 81678 B 256 MB 0.03%
c:/nxp/mcuxpressoide_10.0.0_344/ide/tools/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file C:\Users\M\mcuxpresso\SDKPackages\SDK_2.2_LPCXpresso54608_MCUxpresso\devices\LPC54608\mcuxpresso\libfsl_power_lib_softabi.a(fsl_power_lib.o)
SRAM_0_1_2_3: 23604 B 160 KB 14.41%
SRAMX: 0 GB 32 KB 0.00%
collect2.exe: error: ld returned 1 exit status
USB_RAM: 0 GB 8 KB 0.00%
make: *** [application.axf] Error 1

Have I to download others libraries?

Thanks

标记 (2)
0 项奖励
回复
1 解答
2,837 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Hi Mirko,

we had a problem with the SDK package for LPC546xx such that the soft ABI options wasn't working. A fix is being rolled out in the next few days, so look out for update messages at mcuxpresso.nxp.com.

regards,

Brendon

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,837 次查看
mirko_mancin
Contributor I

New release of SDK released today works!!!

Thanks NXP Team!!

0 项奖励
回复
2,838 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Hi Mirko,

we had a problem with the SDK package for LPC546xx such that the soft ABI options wasn't working. A fix is being rolled out in the next few days, so look out for update messages at mcuxpresso.nxp.com.

regards,

Brendon

0 项奖励
回复
2,837 次查看
mirko_mancin
Contributor I

Thanks for the quick response. I look forward to the next release.

Regards,

Mirko

0 项奖励
回复