Timer0 interrupt.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Timer0 interrupt.

1,798 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lenguyen on Fri Apr 04 13:27:25 MST 2014
Hi All,

I am working on to make a timer0 interrupt at our rate every 1 msec.
Here's my Code:

void Timer0Init(uint32_t timer_freq)
{

/* Enable Timer 0 clock */
Chip_TIMER_Init(LPC_TIMER0);

/* Timer 0 setp for match and interrupt at TIMER0TICKRATE_HZ */
Chip_TIMER_Reset(LPC_TIMER0);
Chip_TIMER_MatchEnableInt(LPC_TIMER0, 1);
Chip_TIMER_SetMatch(LPC_TIMER0, 1, (timer_freq / TIMER0TICKRATE_HZ));
Chip_TIMER_ResetOnMatchEnable(LPC_TIMER0, 1);
Chip_TIMER_Enable(LPC_TIMER0);

/* Enable timer 0 interrupt */
NVIC_ClearPendingIRQ(TIMER0_IRQn);
NVIC_EnableIRQ(TIMER0_IRQn);

}

void TIMER0_IRQHandler(void)
{
        // Toggle GPIO1
        toggle_io1 = ~toggle_io1
        Chip_GPIO_WritePortBit(LPC_GPIO, 5, 2, toggle_io1);


if (Chip_TIMER_MatchPending(LPC_TIMER0, 1)) {
        Chip_TIMER_ClearMatch(LPC_TIMER0, 1);

                // toggle GPIO2               
                toggle_io2 = ~toggle_io2
Chip_GPIO_WritePortBit(LPC_GPIO, 5, 3, toggle_io2);

}
}

Here's what I see on GPIO.
- GPIO P5.2 toggles every 2.5 uSec
- GPIO P5.3 toggles every 1 msec.

I put the break point in timer 0 ISR routine and the timer 0 MCR = 0x18, that makes sense. My question is why the timer 0 ISR comes every 2.5 usec instead of every 1 msec ?

Thanks
LN



标签 (1)
0 项奖励
回复
1 回复

1,475 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Apr 04 17:06:02 MST 2014
Hi, LN,

Try clearing the timer match interrupt before toggle P5.2. You should get both P5.2 and P5.3 at 1ms toggle.

regards,
0 项奖励
回复