Timer Problem (LPC1768)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timer Problem (LPC1768)

1,581 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by expressouser on Sat Jul 12 05:29:17 MST 2014
Hi,

I am having some problem with TIMER, PCLK divider doesn't seem to work. Even if I set the pclk divider to a value different than that of the default value, it seems like the timer uses the default value.

Here is the part where I configure the timer:

pclk_tick = ((double) 1/ ( SystemFrequency/4) ) * 1000; //ms per PCLK tick.  SystemFrequency is at 100MHz.
  // pclk_tick = ((double) 1/ ( SystemFrequency) ) * 1000;     // this part doesnt work.
counter = ((uint32_t) timer->interval) / pclk_tick ;//desired timer interval, in ms, in my code, this is 1.


PowerUp_Peripheral(PCTIMER0);
//Set_Bit(&(LPC_SC->PCLKSEL0), 2); Clear_Bit(&(LPC_SC->PCLKSEL0), 3); //This part doesnt work.
LPC_TIM0->PR = counter; //this will increment the TC everytime the timer->interval expires.
LPC_TIM0->CTCR &= ~(0x3); //TIMER MODE.

and here's the part where I am 'waiting for a delay':

void wait_for_timer(int whichTimer, uint32_t howLong) {
switch (whichTimer) {
case (TIMER_0):
LPC_TIM0->TCR = 0x03;
LPC_TIM0->TCR &= ~(1 << 1);
while (LPC_TIM0->TC != howLong);
LPC_TIM0->TCR = 0x00;
break;
                 .......
                 .......
}


So if I say:

wait_for_timer(TIMER_0, (1000 * 60) ) ;

with PCLK = 0 , (that is dividided by 4), the function returns after 1 minute.

but with PCLK = 1 (that is divided by 1, and with all those parts of the code marked as this part doesn't work), the function returns after 4 minutes (looks like PCLK is still divided by 4).

Any idea what am I doing wrong?
I dont see this problem in RIT.

Thanks.
Labels (1)
0 Kudos
Reply
0 Replies