Time elapsed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Time elapsed

1,919 Views
LArmstrong1985
Contributor III

I use an  LPC11C24, an I want to calculate with accurancy the time elapsed between instruction in my code.

I don't need it only for debug but I need this value in my code. I searched but I haven't found libraries that implement this usual problem. How can I do it? Simple with a timer is right? Do you have sample code or better library for LPC11C24 or similar?

Thank you very much!

Tags (1)
0 Kudos
Reply
1 Reply

1,758 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Fabio Benevento,

    You don't need the lib, it's very simple, just use systick to calculate the code execute time.

    Give you an example from other MCU:

    systick_init();    
    cal_systick_read_overhead();
    systick_disable();

    systick_init();    
    logic_op_demo_with_normalc();
    systick_disable();

uint32_t cnt_start_value;
uint32_t cnt_end_value;
uint32_t overhead;

void systick_init(void)
{
    SYST_CVR = 0x0;    //clear current timer value
    SYST_RVR = 0x00FFFFFF;
    SYST_CSR = SysTick_CSR_CLKSOURCE_MASK | SysTick_CSR_ENABLE_MASK;   
}

void systick_disable(void)
{
    SYST_CSR &= ~SysTick_CSR_ENABLE_MASK;
}

void cal_systick_read_overhead(void)
{
      uint32_t cnt_start_value;
    uint32_t cnt_end_value;
    
    cnt_start_value = SYST_CVR;
 
    cnt_end_value = SYST_CVR;
    
    overhead = cnt_start_value - cnt_end_value;
    
#ifdef DEBUG_PRINT
    printf("systick start value: 0x%x\n\r", cnt_start_value);
    printf("systick end value: 0x%x\n\r", cnt_end_value);
    printf("systick current value read overhead: 0x%x\n\r", overhead);
#endif

}

void logic_op_demo_with_normalc(void)
{
    uint32_t cnt_start_value;
    uint32_t cnt_end_value;
    
    uint32_t execution_cycle;    //actual execution cycle
 
    //configure PTA5 as GPIO
    PORTA_PCR5 = PORT_PCR_MUX(1);
 
    //configure PTA5 as output pin
    GPIOA_PDDR |= 0x20;
 
    cnt_start_value = SYST_CVR;
 
    GPIOA_PDOR ^= 0x20;
 
    cnt_end_value = SYST_CVR;
    
    execution_cycle = cnt_start_value - cnt_end_value - overhead;
    
#ifdef DEBUG_PRINT
    printf("systick start value: 0x%x\n\r", cnt_start_value);
    printf("systick end value: 0x%x\n\r", cnt_end_value);
    printf("actual execution cycle for logic operation with normal C code: 0x%x\n\r", execution_cycle);
#endif        
}

The above example is used to check the GPIOA_PDOR ^= 0x20; execution time.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply