Throughput between SPI and USART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Throughput between SPI and USART

1,704件の閲覧回数
TEMCEFF
Contributor IV

Both protocols are synchronous protocols. But in USART start and stop bits will be there. In SPI need to provide a delay when CS is asserted or de-asserted. 

Which protocol provides max throughput?

ラベル(5)
0 件の賞賛
返信
1 返信

1,641件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Avinash,

I suggest you use the SPI module, from the timing perspective, the synchronous mode of USART module is very similar to that spi module, the USART synchronous mode includes ONE Start bit, one or two STOP bits, but the SPI does not require any additional bits such as Start/Stop bits.

I think the spi module can give max throughput.

The data sheet of LPC55S69 says that the maximum supported bit rate for USART master and slave synchronous mode is 10 Mbit/s. The SPI is 50MBit/S.

pastedImage_1.png

pastedImage_2.png

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信