Through LPC2294HBD / 01 wanted to write an external flash burn. The burning found abnormal. Can read, read by JFLASH wipe. Doubts are as follows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Through LPC2294HBD / 01 wanted to write an external flash burn. The burning found abnormal. Can read, read by JFLASH wipe. Doubts are as follows

Jump to solution
1,512 Views
1263906294
Contributor I

1.LPC2294, P3, [27] WE write so why do you configure the register or invalid?

2.The P3 [27] voltage is 2.3 V. But the ARM end segment is 3.3 V for CSO P1 [0] and P1 [1].

3. but the P3 [27] can be configured to be used for general IO, which can be printed at low and low points, 0 and 3.3 V.

Error for :

Programming failed @ address 0x80000000(item verification error)

              Failed to program target 

              Failed to program and verify target

0 Kudos
Reply
1 Solution
1,402 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Most of the times, it would be required to generate a proper configuration file according to the used external memory. You could take a look at the following links, that may provide useful related information, depending of the hardware, IDE and debug tool:

https://www.lpcware.com/content/forum/help-j-link-program

https://www.embeddedrelated.com/showthread/lpc2000/8706-1.php

http://www.keil.com/forum/6027/

http://forum.segger.com/index.php?page=Thread&threadID=20

https://www.embeddedrelated.com/showthread/lpc2000/35484-1.php

https://www.lpcware.com/content/forum/need-help-programming-external-flash-lpc-link2-board


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,403 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Most of the times, it would be required to generate a proper configuration file according to the used external memory. You could take a look at the following links, that may provide useful related information, depending of the hardware, IDE and debug tool:

https://www.lpcware.com/content/forum/help-j-link-program

https://www.embeddedrelated.com/showthread/lpc2000/8706-1.php

http://www.keil.com/forum/6027/

http://forum.segger.com/index.php?page=Thread&threadID=20

https://www.embeddedrelated.com/showthread/lpc2000/35484-1.php

https://www.lpcware.com/content/forum/need-help-programming-external-flash-lpc-link2-board


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply