This script is designed for working with only a LPC4350 in the JTAG chain.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

This script is designed for working with only a LPC4350 in the JTAG chain.

1,649 次查看
penghaopenghao
Contributor II

编译器 :IAR for arm 7.50

调试器 :lpc-link2

j-link 版本:v6.00

板子是我们自己做的lpc4370的板子

工程使用的是:lpcopen_2_04_keil_iar_nxp_lpclink2_4370

进入调试的时候连接不上板子,出现:

This script is designed for working with only a LPC4350 in the JTAG chain.

确认板子的jtag和调试器链接没有问题。调试器我用LPC4330_Xplorer链接没用问题,请教一下哪里出了问题,初次使用lpc4370.

标签 (1)
0 项奖励
回复
1 回复

1,486 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

LPC-Link2是支持各个LPC系列的MCU,除了LPC2xxx (ARM7) , LPC3xxx (ARM9).

我建议你可以按照这个帖子的方法,更新完固件后,重新调试。

【经验分享】LPC-LINK2 仿真接口使用注意事项 - ARM Cortex-M系列产品 - 恩智浦技术社区 - 手机版 - Powered by Discuz!  
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复