The future of LPC microcontrollers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The future of LPC microcontrollers

1,699件の閲覧回数
sergedemaseneer
Contributor III

What are future plans with the LPC microcontrollers? Is NXP going to continue developping new ones?

ラベル(1)
2 返答(返信)

1,427件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

NXP will continue to support Kinetis and LPC, to provide diversity of solutions to target markets. The existing longevity program for our existing product lines have not been impacted, with more specific information available online.

Thank you again for confidence in our products, portfolio and direction.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,427件の閲覧回数
arimendes
Contributor III

Serge,

  With the release of the LPC546XX, what you should be worried about is with the future of the Kinetis MCUs.

  Compare:

   LPC54606J512BD100E   U$ 4.69   (for 1K units na Mouser)

   180MHZ, 512K flash, 200K ram, ethernet, quad-spi, etc. 

   

   MK64FX512VLL12   U$ 7.20 (for 1K units na Mouser)

   120MHZ, 512K flash, 256K ram, ethernet, etc.

   

   Ari.