The SCT cannot get the input event

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The SCT cannot get the input event

3,318 Views
Tony2k20
Contributor I

I purchased a development board(845MAX) to evaluate the SCT module
1. Output a 100KHz signal from CLKOUT to P0_21 (which can be measured by the oscilloscope)
2. Route P0_20 as SCT_PIN0 and route to SCT_INMUX 0
3. Short-circuit P0.20 and P0.21
4. Set SCT_OUT0 as the test output 0 (The output waveform can be measured using an oscilloscope by simply matching two values)
5. Set SCT_OUT1 as the test output 1 (set 0 to capture the falling edge of IN0 and set 1 to capture the rising edge of IN0)
(the oscilloscope cannot get any waveform , it is OK after the event was changed to match)
6. SCT_IN0 as a clock doesn't work (either in sampling or asynchronous mode), and SCT doesn't work at all when set( When I use async mode, the debug probe cannot detect the target chip, I erase the flash via ISP and set others clock mode, the IDE can work normally)

I have read the AN11538,  INSYNC should be set to 1, so I do.

Plz help me! 

Thanks

 

const sctimer_config_t SCT0_initConfig = {
.enableCounterUnify = true,
.clockMode = kSCTIMER_System_ClockMode,
.clockSelect = kSCTIMER_Clock_On_Rise_Input_0,
.enableBidirection_l = false,
.enableBidirection_h = false,
.prescale_l = 0U,
.prescale_h = 0U,
.outInitState = (uint8_t)(0),
.inputsync = (1 << 0U)|
};
uint32_t SCT0_event[5];

static void SCT0_init(void)
{
SCTIMER_Init(SCT0, &SCT0_initConfig);
/* Initialization of state 0 */
SCTIMER_CreateAndScheduleEvent(SCT0, kSCTIMER_MatchEventOnly, 1, kSCTIMER_Out_0, kSCTIMER_Counter_U, &SCT0_event[0]);
SCTIMER_SetupOutputClearAction(SCT0, kSCTIMER_Out_0, SCT0_event[0]);

SCTIMER_CreateAndScheduleEvent(SCT0, kSCTIMER_MatchEventOnly, 6, kSCTIMER_Out_0, kSCTIMER_Counter_U, &SCT0_event[1]);
SCTIMER_SetupOutputSetAction(SCT0, kSCTIMER_Out_0, SCT0_event[1]);

SCTIMER_CreateAndScheduleEvent(SCT0, kSCTIMER_MatchEventOnly, 16, kSCTIMER_Out_0, kSCTIMER_Counter_U, &SCT0_event[2]);
SCTIMER_SetupCounterLimitAction(SCT0, kSCTIMER_Counter_U, SCT0_event[2]);

SCTIMER_CreateAndScheduleEvent(SCT0, kSCTIMER_InputFallEvent, 0, kSCTIMER_Input_1, kSCTIMER_Counter_U, &SCT0_event[3]);
SCTIMER_SetupOutputClearAction(SCT0, kSCTIMER_Out_1, SCT0_event[3]);

SCTIMER_CreateAndScheduleEvent(SCT0, kSCTIMER_InputRiseEvent, 0, kSCTIMER_Input_1, kSCTIMER_Counter_U, &SCT0_event[4]);
SCTIMER_SetupOutputSetAction(SCT0, kSCTIMER_Out_1, SCT0_event[4]);

SCTIMER_StartTimer(SCT0, kSCTIMER_Counter_U);
}

void BOARD_InitPins(void)
{
/* Enables clock for IOCON.: enable */
CLOCK_EnableClock(kCLOCK_Iocon);
/* Enables clock for switch matrix.: enable */
CLOCK_EnableClock(kCLOCK_Swm);
/* SCT_PIN0. Assign to pin using the switch matrix 0 */
INPUTMUX_AttachSignal(INPUTMUX, 0U, kINPUTMUX_SctPin0ToSct0);

const uint32_t DEBUG_UART_RX = (/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Enable hysteresis */
IOCON_PIO_HYS_EN |
/* Input not invert */
IOCON_PIO_INV_DI |
/* Disables Open-drain function */
IOCON_PIO_OD_DI |
/* Bypass input filter */
IOCON_PIO_SMODE_BYPASS |
/* IOCONCLKDIV0 */
IOCON_PIO_CLKDIV0);
/* PIO1 PIN16 (coords: 36) is configured as USART0, RXD. */
IOCON_PinMuxSet(IOCON, IOCON_INDEX_PIO1_16, DEBUG_UART_RX);

const uint32_t DEBUG_UART_TX = (/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Enable hysteresis */
IOCON_PIO_HYS_EN |
/* Input not invert */
IOCON_PIO_INV_DI |
/* Disables Open-drain function */
IOCON_PIO_OD_DI |
/* Bypass input filter */
IOCON_PIO_SMODE_BYPASS |
/* IOCONCLKDIV0 */
IOCON_PIO_CLKDIV0);
/* PIO1 PIN17 (coords: 37) is configured as USART0, TXD. */
IOCON_PinMuxSet(IOCON, IOCON_INDEX_PIO1_17, DEBUG_UART_TX);

/* USART0_TXD connect to P1_17 */
SWM_SetMovablePinSelect(SWM0, kSWM_USART0_TXD, kSWM_PortPin_P1_17);

/* USART0_RXD connect to P1_16 */
SWM_SetMovablePinSelect(SWM0, kSWM_USART0_RXD, kSWM_PortPin_P1_16);

/* CLKOUT connect to P0_21 */
SWM_SetMovablePinSelect(SWM0, kSWM_CLKOUT, kSWM_PortPin_P0_21);

/* SCT_PIN0 connect to P0_20 */
SWM_SetMovablePinSelect(SWM0, kSWM_SCT_PIN0, kSWM_PortPin_P0_20);

/* SCT_OUT0 connect to P1_21 */
SWM_SetMovablePinSelect(SWM0, kSWM_SCT_OUT0, kSWM_PortPin_P1_21);

/* SCT_OUT1 connect to P1_20 */
SWM_SetMovablePinSelect(SWM0, kSWM_SCT_OUT1, kSWM_PortPin_P1_20);

/* Disable clock for switch matrix. */
CLOCK_DisableClock(kCLOCK_Swm);

}

 

 

0 Kudos
Reply
6 Replies

3,300 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello

5. Set SCT_OUT1 as the test output 1 (set 0 to capture the falling edge of IN0 and set 1 to capture the rising edge of IN0)(the oscilloscope cannot get any waveform

>>It seems you use config tool to generate code, so how about create a new project, that just test this function, give a signal to IN0 not from SCT, for example just a high to low to high, check whether the SCT_OUT1 can work well.

 

Regards,

Alice

 

 

0 Kudos
Reply

3,291 Views
Tony2k20
Contributor I

The pin configuration is as follows

Tony2k20_0-1605171536169.pngTony2k20_0-1605171536169.png

If there is any problem, could you please point it out

0 Kudos
Reply

3,280 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

You can share your  project, I help to check my side, thanks!

 

Regards,

Alice

 

0 Kudos
Reply

3,277 Views
Tony2k20
Contributor I

Thank you

I think I've found the problem! It is OK now. 

INPUTMUX_Init(INPUTMUX) should be executed before the INPUTMUX setting.

CLOCK_EnableClock(kCLOCK_Sct);
CLOCK_EnableClock(kCLOCK_Dma);

In this function: The inputmux clock of sct  is enabled.

The SCT INMUX clock is drived by xxx? CLOCK_SCT or CLOCK_SWM ?

 

 

0 Kudos
Reply

3,265 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

I think is CLOCK_SCT,  there is no mentioned clearly, while need enable SCT clock then can

control  the INPUTMUX register.

 

Regards,

Alice

0 Kudos
Reply

3,298 Views
Tony2k20
Contributor I

I have set SCT_IN4( SCT_CLK  == 200kHz ) as the SCT input, the input event can work normally.

The problem may lie in the input Settings for the SCT.

Could you show me an example of SCT input Settings?

0 Kudos
Reply