The Lpc4330 can’t boot from spifi flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Lpc4330 can’t boot from spifi flash

1,680件の閲覧回数
pengdacheng
Contributor I

I am using the OM13027: LPC4330-Xplorer Board,which I can found that it is flashless and  use the external flash S25FL032P0XMFI013. I download some example project from nxp websit and generate the binary files. After I program the external flash and turn off the power, when I repower the board the lpc4330 can not boot from the spifi flash.  I had set the boot mode right but I don't know why it can't still boot from external flash.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,559件の閲覧回数
miguel_mendoza
NXP Employee
NXP Employee

Hi peng dacheng,

Could you give me more information about what example are you trying to prove, are you using the LPCOpen examples?

regards,
Miguel Mendoza

0 件の賞賛
返信