Testing CAN loopback mode on LPC1857.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Testing CAN loopback mode on LPC1857.

768 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pavan_munavalli on Tue Oct 28 13:36:28 MST 2014
Hello All,

I have a problem testing the loop back mode for CAN controller on LPC1857. I am using the can example of LPCopen. I am able to successfully transmit the message. The status register value after the transmission is "1000" which indicates that the transmission is successful. I am having problems knowing whether the transmitted message has come back again. The status register also does not indicate whether a new message has been received.

Can anyone please tell me how to check whether the transmitted message has been received back.

Thanks.
标签 (1)
0 项奖励
回复
0 回复数