Target Reset Pattern

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Target Reset Pattern

Jump to solution
1,735 Views
lb_h
Contributor I

Hello,all

Can the I3C module of the LPC55xx family of chips send a "Target Reset Pattern" through a configuration register?Whether the T-bit of the I3C command is automatically calculated by the hardware or can be configured by software.

Labels (1)
0 Kudos
Reply
1 Solution
1,701 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @lb_h 

In the LPC55xx family, the I3C module does not have a dedicated configuration register to directly send the “Target Reset Pattern.” However, it supports sending custom command sequences, which can be used to generate the reset pattern manually by software.

The T-bit is typically calculated automatically by the hardware based on the I3C command.

BR

Harry

View solution in original post

0 Kudos
Reply
1 Reply
1,702 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @lb_h 

In the LPC55xx family, the I3C module does not have a dedicated configuration register to directly send the “Target Reset Pattern.” However, it supports sending custom command sequences, which can be used to generate the reset pattern manually by software.

The T-bit is typically calculated automatically by the hardware based on the I3C command.

BR

Harry

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-1998675%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ETarget%20Reset%20Pattern%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1998675%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHello%2Call%3C%2FP%3E%3CP%3ECan%20the%20I3C%20module%20of%20the%20LPC55xx%20family%20of%20chips%20send%20a%20%22Target%20Reset%20Pattern%22%20through%20a%20configuration%20register%3FWhether%20the%20T-bit%20of%20the%20I3C%20command%20is%20automatically%20calculated%20by%20the%20hardware%20or%20can%20be%20configured%20by%20software.%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1998675%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3ELPC55xx%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2000807%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20Target%20Reset%20Pattern%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2000807%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F239137%22%20target%3D%22_blank%22%3E%40lb_h%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3EIn%20the%20LPC55xx%20family%2C%20the%20I3C%20module%20does%20not%20have%20a%20dedicated%20configuration%20register%20to%20directly%20send%20the%20%E2%80%9CTarget%20Reset%20Pattern.%E2%80%9D%20However%2C%20it%20supports%20sending%20custom%20command%20sequences%2C%20which%20can%20be%20used%20to%20generate%20the%20reset%20pattern%20manually%20by%20software.%3C%2FP%3E%0A%3CP%3EThe%20T-bit%20is%20typically%20calculated%20automatically%20by%20the%20hardware%20based%20on%20the%20I3C%20command.%3C%2FP%3E%0A%3CP%3EBR%3C%2FP%3E%0A%3CP%3EHarry%3C%2FP%3E%3C%2FLINGO-BODY%3E