TRST - Pullup, pulldown or floating ? [ Custom PCB]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TRST - Pullup, pulldown or floating ? [ Custom PCB]

1,072 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fnp-intellegre on Thu Nov 06 11:02:07 MST 2014
Using the LPC1833 TFBGA 100 Pin package I have the 6pin Tag Connect TC-2030 Cortex SWD debug connector connected to the part.
Does TRST need to be pulled up even though it is not being used ?
标签 (1)
0 项奖励
回复
1 回复

1,032 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Nov 06 12:34:35 MST 2014
The TRST pin has an internal pull-up, so an external pull-up is not required.

Paul
0 项奖励
回复