TDA8026 - Card Activation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TDA8026 - Card Activation

5,217件の閲覧回数
thiago_machado
Contributor III

Hello all. I'm currently working on a Contact Card Interface. The idea is to send APDU's from a i.MX8M microprocessor throught it's USB bus to PN7412, that has a TDA8026 connected to it. I was able to successfully communicate and activate contact cards located at PN main slot, but when I try to replicate the same procedure in a card located at one of the TDA8026 slots (Slot 5), I get a empty ATR vector response, meaning that no activation was done. Here's the steps I followed in order to make it respond.

    phStatus_t eStatus = PH_ERR_FAILED;
#ifdef PHFL_ENABLE_SAM_KEY_STORE
    /* Global instance for  CT pal parameter's structure */
    phhalCt_InitParam_t sInitParams;
    uint8_t gbAtrBuffer[32]={0};
    phpalCt_DataParams_t tDataParams;
	tDataParams.pbAtrBuffer = (uint8_t *)&gbAtrBuffer;
	tDataParams.bSizeOfATRbuffer = 32;

    sInitParams.bAutoCTDeactivationEnable= 0;
    sInitParams.bCardPresConnectorStatus= gpkphCfg_EE_Boot_CT->bConnectorType;
    sInitParams.bPullupSetStatus = gpkphCfg_EE_Boot_CT->bPullUp;
    sInitParams.bSlewRateConfig = gpkphCfg_EE_Boot_CT->bSlewRate;

    phpalCt_Init(&sInitParams);

    do
   {
        tDataParams.pbAtrBuffer = (uint8_t *)&gbAtrBuffer;
        tDataParams.bSizeOfATRbuffer = 32;

       /*Initialize the TDA*/
       eStatus = phhalTda_Init();
       CHECK_SUCCESS(eStatus);

       /*Switch to auxiliary slot, because SAM is will be used from auxiliary slot*/
       phhalCt_SwitchSlot(E_AUXILIARY_SLOT);

       /*Select the Auxiliary slot number*/
       eStatus = phhalTda_SelectSlot((uint32_t)gbTdaSlotNum);

       /*Check the presence of SAM in the selected slot*/
       eStatus = phhalTda_GetStatus(E_PRESENCE);
       if(eStatus != SAM_CARD_PRESENT_IN_SLOT)
       {
           break;
       }

    phpalCt_SetConfig(E_EMV_ENABLE,0);


    /*Activate the SAM card*/
    eStatus =  phhalTda_ActivateCard(&tDataParams);

I'm using DoorAcceessExample_AUX_slot software example provided by NXP and developed by Anish Ahammed in 2016.

タグ(3)
7 返答(返信)

4,732件の閲覧回数
davidsagasta97
Contributor I

Hi! is there any axample/code that initialites any TDA, using GPIO instead of I2C? some TDAs doesnt have an I2C interface. Thanks!

0 件の賞賛
返信

4,893件の閲覧回数
tyugayNA
Contributor I

Hello! How to get DoorAcceessExample_AUX_slot example? How I can request it? Where do I need to sign valid NDA?

0 件の賞賛
返信

5,175件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @thiago_machado ,

 

Did you make any change in DoorAcceessExample_AUX_slot example? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

5,167件の閲覧回数
Bonat
Contributor I


@Kan_Li Where is this example? I can't find it.

0 件の賞賛
返信

5,145件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Bonat ,

 

It is part of EC version but not publicly released , you may request it via the following channel with a valid NDA. Please kindly refer to the following for details.

 

https://community.nxp.com/t5/HomeTest-Knowledge-Base/How-to-submit-a-new-question-for-NXP-Support/ta...

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

5,087件の閲覧回数
Bonat
Contributor I

Thank you for your reply, Kan Li! Could you give me access to this content? I got this message when i tried to access: "You do not have sufficient privileges for this resource or its parent to perform this action."

Best regards,

Bruno.

0 件の賞賛
返信

5,062件の閲覧回数
Bonat
Contributor I

@Kan_Licould you help me with this?

0 件の賞賛
返信