System clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

System clock

1,396 次查看
zhan8g
Contributor I

It is found that there is a problem in the LPC54102 chip. The internal IRC 12MHz clock is passed through EMI, but IRC has the problem of temperature drift. The long-term usage leads to UART communication rate deviation and can not communicate. Using 32K RTC PLL TO 12MHz, the system clock temperature drift problem has been solved, but there are more serious problems and very poor anti-interference. Why does this chip have such a problem?!!

标签 (1)
0 项奖励
回复
1 回复

1,296 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

I'd like to get the more detailed information about this issue, so whether you can introduce the process of testing and tell me the device revision number of this LPC54102 chip.

Have a great day.

TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 项奖励
回复