System clock divider register = 1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

System clock divider register = 1?

2,663件の閲覧回数
vaque
Contributor II

Hi!;

I was trying putting a LPC824 System clock divider register = 1 (UM10800 5.6.13 System clock divider register) with IRC Oscillator asociated main clock for the maximum speed.

If I try it with a LPCXpresso824-MAX development board, lpcxpresso doesn't debug and if i program it by the ISP, the UART it works badly.

Why is it?????

Thanks and regards. Daniel.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,096件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Daniel Vaquerizo,

    After modify the SYSAHBCLKDIV =1, I can use the LPCXpresso 824 MAX to debug in LPCXpresso IDE, this is the test result:

pastedImage_1.png

The code is the lpcopen_2_19_lpcxpresso_nxp_lpcxpresso_824.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,096件の閲覧回数
vaque
Contributor II

Hi.

Thats weird... i only do this:

foro1.pngforo2.png

Regards and thanks so mucho. Daniel.

0 件の賞賛
返信

2,096件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Daniel,

    After you modify the divider, please add some delay to wait the clock stable.

   Please try it again, if you still have problem, please send me your test project, I will check it on my side.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信