SwdRead: Timeout waiting for response_"LPC55s28"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SwdRead: Timeout waiting for response_"LPC55s28"

1,374 Views
Trada94
Contributor I

Hello community,

I have the following issue when I trying to lock the MCU LPC55sXX. Unit ng.png

I am following these steps to lock the MCU:

1.- Configure the MCU in ISP mode.

2.- Write the bin file to the CFPA.

3.- Write the bin file to the CMPA.

4.- Verify if the MCU is locked and expected the following result: Unit good.png

The issue occurs intermittently.

Any help would be greatly appreciated. 

 

0 Kudos
Reply
3 Replies

1,334 Views
Trada94
Contributor I

Hello @Alice_Yang 

I am trying to understand the functions of CMPA and CFPA. 

Could you please explain what they are?

Thanks, I really appreciate your help

AE

0 Kudos
Reply

1,298 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Trada94 

CMPA (Configuration Memory Protection Area) and CFPA (Code Flash Protection Area) are mainly used to store security-related configuration information and provide protection functions for memory areas.

For details, please refer to "Chapter 10: LPC55S6x/LPC55S2x/LPC552x Protected Flash Region" of UM11126.

 

BR

Alice

0 Kudos
Reply

1,362 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Trada94 

To disable the ISP and SWD of LPC55xx, please refer to
 
BR
Alice
0 Kudos
Reply