Supported SPI Flash Chips for the LPC4350

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supported SPI Flash Chips for the LPC4350

1,547 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Mon Mar 10 08:38:49 MST 2014
On our product using the NXP LPC4350FET256, we are currently using a 150 mil SOIC-8 SPIFI Flash chip:  Winbond W25Q80BVSNIG (8Mbit).  This chip is going end of life and we would like to find an alternative with the same package but larger memory size - at least 16Mbit but preferably 32 Mbit.  I can’t find a part that matches the package size on the standard list in the user manual for the LPC4350.  Is there a more extensive list available than what’s in the user manual, or does anyone have any recommendations?

From research I am looking at the following possibilities, do you know if any of these are compatible with the boot ROM code.  I am hoping that they will boot properly and be configured to operate at the highest speed without any further configuration after boot ROM startup.

Spansion
S25FL132K0XMFI043(32Mbit)
S25FL116K0XMFI043(16Mbit)

Winbond
W25Q16DVSNIG(16Mbit)

Macronix
MX25U1635EM1I-10G(16Mbit)


Labels (1)
0 Kudos
Reply
3 Replies

1,478 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Wed Mar 12 11:56:52 MST 2014
Thanks for the information!

Greg
0 Kudos
Reply

1,478 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Wed Mar 12 08:58:22 MST 2014
I currently am not able to confirm that the following will work, however, the boot-ROM was modified so they should officially be bootable. The prices of these are quite low.

Micron makes two different sizes:
Narrow:
  N25Q032ESC
Wide:
  N25Q032ESE

0 Kudos
Reply

1,478 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Mar 10 15:53:07 MST 2014
Hi Greg,
Following device will work.

Macronix(MXIC)  MX1635E

Winbond: 25Q16DV,25Q32FV
0 Kudos
Reply