Stuck in while (!(LPC_SYSCON->SYSPLLCLKUEN & 0x01)); /* Wait Until Updated */

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Stuck in while (!(LPC_SYSCON->SYSPLLCLKUEN & 0x01)); /* Wait Until Updated */

1,769 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Scribe on Tue Nov 27 11:38:14 MST 2012
Hi guys,

I've been attempting to implement basic SPI flash in the mass sotrage example for 11Uxx in 0.98/a for a while, however find that whenever I include my flash file and call the setup function I get stuck in the following setup loop:

while (!(LPC_SYSCON->SYSPLLCLKUEN & 0x01));     /* Wait Until Updated       */

What's making me lose my mind is that this loop should execute before any code as it's from system_LPC11UXX.c I don't have a clue how I got here. If I attempt to insert break-points it doesn't help, I get stuck here before I even reach the new code.

On the off chance this was a RAM space issue, I reduced a large memory structure in another file considerably to no avail, my new code doesn't use that much RAM so this seems unlikely...


I'm baffled guys, any idea?
标签 (1)
0 项奖励
回复
1 回复

1,140 次查看
tangtang78
Contributor I

You may have used software simulator instead of a hardware emulator. If so, you can add an initialization file with the content "map 0x40000000,0x400FFFFF read write".

0 项奖励
回复