Starting with the GLCD 240x128 with LPC1768 microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Starting with the GLCD 240x128 with LPC1768 microcontroller

2,514 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Homayon on Wed Jul 02 04:42:37 MST 2014
I'm using 240x128 and LPC1768. Do you have a library for this LCD? Or sample code to use it?
Chipset's LCD: T6963C
If you have access to the schematic, I give thanks.

[img]http://roboeq.ir/uploads/images/shop/products/L13345337839250.jpg[/img]

Labels (1)
0 Kudos
Reply
3 Replies

2,130 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Jul 02 13:32:48 MST 2014
Hi Homayon,
emWin  has Display Driver GUIDRV_SLin which supports T6963. Do not know how different is T6963C from T6963?  We have BSP examples for our microcontroller not exactly same driver but may be useful to you see below link.

http://www.lpcware.com/content/nxpfile/nxpemwin514mcb1700bsp

Here is full emWin library/BSP page
http://www.lpcware.com/content/project/emwin-graphics-library
0 Kudos
Reply

2,130 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Homayon on Wed Jul 02 13:14:50 MST 2014
Thank you. I've looked at this thread.
I'm looking for a rich library for this LCD but I can not find anything to the microcontroller.
The only way left for me is that my libraries Codevision to become Keil
0 Kudos
Reply

2,130 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Jul 02 10:08:00 MST 2014
Hi Homayon,
There is some information here which may help you. I did not test it though.
http://www.lpcware.com/content/forum/t6963c-graphic-lcd
0 Kudos
Reply