Source code of I2C-util.exe for secondary I2C bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source code of I2C-util.exe for secondary I2C bootloader

1,620 Views
MartinHo
Contributor IV

Is it possible to get the source code of the I2C-util.exe incuded in AN11780?

best regards

martin

Labels (1)
0 Kudos
Reply
1 Reply

1,572 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Martin, 

Unfortunately, is not possible to get the source code of this application. I apologize for the inconvenience that it might cause you. 

Regards,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

0 Kudos
Reply