Source Code for AN11365 CMOS Camera Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source Code for AN11365 CMOS Camera Interface

3,333 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Thu Feb 06 17:14:01 MST 2014
Is there source code available to go along with the CMOS camera interface app note AN11365?

Thanks,
Labels (1)
0 Kudos
Reply
5 Replies

3,230 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Apr 24 20:20:04 MST 2015
Hi Anthony,
You can buy it from Digikey and Mouser see below links
http://www.digikey.com/product-detail/en/OM13059UL/568-11367-ND/4743658?WT.z_cid=sp_568_buynow

http://www.mouser.com/ProductDetail/NXP/OM13059UL/?qs=%2fha2pyFaduivyg0n0nASJHRmsyjuDSiy4FEuKCPr0wfH...

0 Kudos
Reply

3,230 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embedded_guy on Wed Feb 04 14:42:29 MST 2015
Hi Wouter,

I am looking to purchase the OM13059 development kit, or at least the add-on board and camera (SGPIO and SCT Camera Interfaces). Where can I find this? The app note points to this site.

Thanks,
Anthony
0 Kudos
Reply

3,230 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dsidlauskas on Sun Feb 09 12:37:22 MST 2014
Awesome. Thank you very much.
0 Kudos
Reply

3,230 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Fri Feb 07 06:41:07 MST 2014
Hi David,

The source code is included in the following .zip file: http://www.lpcware.com/content/nxpfile/an11365-sct-camera-interface-design-lpc1800-and-lpc4300

Regards,
Wouter
0 Kudos
Reply

3,230 Views
maneesh_pawar
Contributor I

Unable to download.

Kindly make it available.

regards

0 Kudos
Reply