Some problems getting started

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some problems getting started

1,208 Views
maza
Contributor I

Hello!

In my company was working some employee who destroyed the LPCXpresso824 max board that I'm using now and of course, its giving me some headaches.

To begin, I tried to build and load the blink example but didn't work. Then I realize that I probably should reflash the firmware by updating a new binary file... okey, tried an didn't work. I pressed the reset button while pluggin in the usb connector but nothing happens and my devide manager doesn't detect anything, is this right? Shouldn't the device manager show a new device called CRP DISABLD as the guide says?

To make it easier, it's my very first time programming MCU, not counting Arduino. So i'm too lost to start without any help.

Could you help me? 

Thanks

0 Kudos
Reply
1 Reply

1,118 Views
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following link, you will find a way to recover the board getting it into ISP mode.

Regaining debug access to target MCU 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply