Smallest programing size on LPC5500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Smallest programing size on LPC5500

Jump to solution
4,309 Views
JRIIS
NXP Employee
NXP Employee

I need to understand what is the smallest bit size that can be programmed - within one operation - in internal Flash on LPC5528.

I also need to understand what is the smallest size that be erased at one operation.

This file is for collecting and store calibration data from production/test, but need to be passable to update a few times over product lifetime after reparation.

 Thanks,

/Jakob

Labels (1)
0 Kudos
Reply
1 Solution
4,298 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi JRIIS 

It's right the minimum programming and erase size is the page size, 512 bytes. The HW decides this feature. No other option.

Hope this clarifies the issue.

Jun Zhang

View solution in original post

0 Kudos
Reply
2 Replies
4,304 Views
JRIIS
NXP Employee
NXP Employee

I found following my self:

2.1.1 Page size and sector size

The sector size of the LPC5500 series internal flash memory is 32 KB and the page size is 512 bytes.

The minimum programming size is the page size, 512 bytes.

The minimum erase size is page size, 512 bytes

AN12949 where I found this info is attached.

This seem to be quite large potion - so if there is any tip to program smaller potion? then I like to know.

Thanks,

Jakob

0 Kudos
Reply
4,299 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi JRIIS 

It's right the minimum programming and erase size is the page size, 512 bytes. The HW decides this feature. No other option.

Hope this clarifies the issue.

Jun Zhang

0 Kudos
Reply